How to assemble a RX-28 and RX-64 together.
페이지 정보
10-09-13 16:07 Hit 8,620There are many ways you can assemble the RX-28 and RX-64 together.
The RX-28 is the top-most servo, and the RX-64 is immediately beneath it.
Below are the frames required to assemble them together.
1) RX-24F/RX-28 FR07-B101K Set
2) RX-64/EX-106+ FR05-S101 Set OR RX-64/EX-106+ FR05-S101K Set
Please refer to the links below to get more information on assembly.
1) RX-28 Assembly.
http://emanual.robotis.com/docs/en/dxl/rx/rx-28/
2) RX-64 Assembly.
http://emanual.robotis.com/docs/en/dxl/rx/rx-64/





サポート