...

チュートリアル

Changing the Dynamixel's ID

페이지 정보

10-09-08 11:49 Hit 10,183

Changing the ID using the CM-2+ and CM-5

1. Changing the ID using the CM-5(Same applies for the CM2+)

Connect just one Dynamixel to the CM-5 which you wish to change the ID of.
Download the Behavior Control Program to change the Dynamixel’s ID.
After downloading the program, execute the program using the ID changing.wvm.
Use the buttons on the CM-5 to set the newly set ID. (Refer below)
Once the desired ID has been set, close the program.

Please refer to the ID changing.wvm video which can be found in the CD.

Please refer to the below when changing the Dynamixel’s ID.

- If you press the U button on the CM-5, the new ID will increase by 1.
- If you press the D button on the CM-5, the new ID will decrease by 1.
- If you press the L button on the CM-5, the new ID will increase by 10.
- If you press the R button on the CM-5, the new ID will decrease by 10.
- If you press the START button on the CM-5, the old ID will change to the new ID.


AX-12+ uses IDs 0~30 and AX-S1 uses 100~109.


2. Changing the ID using Robot Terminal

Connect your Dynamixel to the CM-5
Press the MODE button to move the LED to Manage Mode. Then, press START.
For a normal case, it will show the IDs of the connected Dynamixels.
If the currently connected Dynamixel does not show up, use the search command to find the Dynamixel. (Refer to search ID and communication speed)
Make a communicable environment for the connected Dynamixels using the 'cid (ID)' command.

 

1.jpg

 

You can change to the desired ID using the 'w 3 (ID)' command. The example below is changing to ID #2.

 

2.jpg

 

If you press the MODE button and then press the START button to execute the program, you can find the replaced Dynamixel.

 

3.jpg  

 

 

Changing the ID using RoboPlus Terminal

 

4.jpg  

 

Click here for details. 

 

 

  • 페이스북으로 보내기
  • 트위터로 보내기
  • 구글플러스로 보내기