Modifying your humanoid’s actuator offset
페이지 정보
10-09-09 15:07 Hit 7,874Modifying your humanoid’s actuator offset
Unlike the example, humanoid walk on two feet, and because balance affects this robot a lot, it is difficult to get the correct offset. It is very unlikely that you’ll be able to solve this problem with the example programs. You will have to set it a couple of times, to get the proper balance.
Here a few tips!
- Please refer to page 206~208. Be sure to set the same or similar offset as in the figure.
- The robot’s left and right angle must be alike. When looking at its angle, look at front, back, left and right side.
- Turn the robot around to see if the foot is even. Using a ruler will help.
- Instead of having its upper body be vertical with the ground, stooping a bit will help.
- Spreading its legs a bit and bring the hip down a bit will make its walk more stable.
- When the robot falls forward or backward, do not modify the entire leg movement. Simply modify the ankle (ID# 15 and 16) and pelvis (ID# 11 and 12)
- If the robot leans too much to the left or right when walking, turn off the actuator (ID 9, 10, 17, and 18) that move sideways.
- When the robot balance has been messed up after too much offsetting, instead of fixing it use the default motion and modify it.





サポート