[S/W update] R+ Motion 2.0 (v2.2.3)
페이지 정보
2015/02/06 16:06 Hit 14,226본문
Some bugs were found in the recent update for R+ Motion in January (v2.2.2).
The latest version v.2.2.3 has been released to solve the issues.
Bug : Wired downloading bug
1. OS : Windows
The latest version v.2.2.3 has been released to solve the issues.
Bug : Wired downloading bug
1. OS : Windows
2. Problem : High rate of failure when downloading with LN101, USB2Dynamixel, Mini USB on R+ Motion v2.2.2.
- There is no problem with BT-210 or BT-110.
- v.2.2.2 has faster downloading speed, which causes the problem.
3. Solution : Please run the auto-update when you run the R+ Motion program, to update to v.2.2.3.
4. Also updated : When searching for a Bluetooth module on Windows, only one port will be searched (instead of 2).
- There is no problem with BT-210 or BT-110.
- v.2.2.2 has faster downloading speed, which causes the problem.
3. Solution : Please run the auto-update when you run the R+ Motion program, to update to v.2.2.3.
4. Also updated : When searching for a Bluetooth module on Windows, only one port will be searched (instead of 2).





Company