...

お知らせ

[S/W update] R+ Motion 2.0 (v2.2.3)

페이지 정보

2015/02/06 16:06 Hit 14,243

본문

Some bugs were found in the recent update for R+ Motion in January (v2.2.2).

The latest version v.2.2.3 has been released to solve the issues.



Bug : Wired downloading bug



1. OS : Windows

 
2. Problem : High rate of failure when downloading with LN101, USB2Dynamixel, Mini USB on R+ Motion v2.2.2.

   - There is no problem with BT-210 or BT-110.

   - v.2.2.2 has faster downloading speed, which causes the problem.

               

3. Solution : Please run the auto-update when you run the R+ Motion program, to update to v.2.2.3.



4. Also updated : When searching for a Bluetooth module on Windows, only one port will be searched (instead of 2).

  • 페이스북으로 보내기
  • 트위터로 보내기
  • 구글플러스로 보내기